{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.

Search FAQs

How to add TM5SAO4 H/L close to a "high power module" on a TM5NCO1 CANopen island ?

According to documentation TM5SAO4 H/L can not be mounted close to TM5 slices dissipating more than 1.15 W ("high power module" like TM5SPS3) when ambient temperature is more than 55°C.
In this case dummy modules are needed in-between.
But is it OK to do that when ambient temperature is lower than 55°C.

Unfortunalely SoMachine DTM for TM5NCO1 does not take ambient temperature into account and considers worse case only ( > 55°C).

If ambient temperature around your island is lower than 55°C then you can use TM5SAO4 H/L close to modules with power dissipation > 1.15 W. Follow these steps to build your island with SoMachine :
- start with an empty island : TM5SPS3 only
- add a dumy module
- add a TM5SAO4 H/L
- remove the dummy module : an error pop-up appears : simply ignore it.

Schneider Electric Nigeria

Explore more
Range:
Modicon M258Modicon TM5 IP20 modular I/O system
Explore more
Range:
Modicon M258Modicon TM5 IP20 modular I/O system
Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.