{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.

Search FAQs

Where do I find information on electrolyte contained within the SYBTU1-PLP and SYBTU2-PLP type APC, and/or the SE modular batteries such as GVSBTU, GVSBTHU and GVSBTHULL

Article available in these languages: Spanish

Issue:
Where to find information on electrolyte contained within the SYBTU1-PLP and SYBTU2-PLP type APC modular batteries, and/or the SE modular batteries such as GVSBTU, GVSBTHU and GVSBTHULL


Product line:
SYBTU1-PLP / SYBTU2-PLP, GVSBTU/GVSBTHU/GVSBTHULL


Environment:
PX1,2, 250-500, SUVT, Galaxy 3500, Galaxy VS


Information:
See application note 143 for specific values of contained electrolyte in both the SYBTU1-PLP (used in PX1 20,40, 48, 80 and 96KVA UPS units as well as the SUVT and Galaxy 3500 UPS units) and the SYBTU2-PLP (used in the PX2 100KVA and the PX 250/500KVA UPS units) batteries.

Application Note 143:
http://www.apc.com/salestools/SMCR-6NXGXU/SMCR-6NXGXU_R2_EN.pdf


Note – SYBTU1-PLP and SYBTU2-PLP use batteries manufactured by four different vendors. For further information on MSDS by the specific vendors please refer to FA157067

Also see FA157067

Galaxy VS Modular Batteries:
Battery TypeElectrolyte WeightElectrolyte Volume
(kg)(lbs)(ml)(gal)
GP1272F2FR0.51.113780.1
HR1234WF2FR0.440.983330.09
UP-PW1245P10.47941.0573780.0998
Battery TypeElectrolyte WeightElectrolyte Volume
(kg)(lbs)(ml)(gal)
GVSBTU511.137801
GVSBTHU4.49.833300.9
GVSBTHULL4.79410.5737800.998
Battery TypeElectrolyte WeightElectrolyte Volume
(kg)(lbs)(ml)(gal)
GVSBT42044.4151204
GVSBTH417.639.2133203.6
GVSBTH4LL19.17642.28151203.992

Schneider Electric Nigeria

Attachment(s)

Galaxy VS Modular Battery MSDS.pdfGalaxy VS Modular Battery MSDS.pdf [238 KB]
Explore more
Range:
Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.
Explore more
Range: