{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
Search FAQs
Can the sliding doors from HyperPod be used on an EcoAisle?
Issue:
Can EcoAisle doors be used with a HyperPod.

Product Line:
EcoAisle, HyperPod

Environment:
All versions and serial ranges

Cause:
The sliding doors used with HyperPod are very cost-effective.

Resolution:
The first release of the HyperPod, are not compatible with EcoAisle.  HyperPod doors do not adapt to EcoAisle.  There are no plans currently to make them fit.

Schneider Electric Nigeria