Search FAQs
Why can't I change most settings on my Altivar Drive?
Issue:
Customer can not make parameter changes on Altivar Drive.
Product Line:
Altivar Drive
Environment:
All serial numbers for Altivar Drive
Cause:
Cannot make any changes to the drive
Resolution:
Customer can not make parameter changes on Altivar Drive.
Product Line:
Altivar Drive
Environment:
All serial numbers for Altivar Drive
Cause:
Cannot make any changes to the drive
Resolution:
- The most common reason is because the drive is running
- If the drive is running, most parameters are locked and cannot be changed until the drive is stopped
- Altivar Process Drive, ATV61/71
- Check Drive Status on top left corner
- ATV312, ATV32, ATV12
- Check main display. If it shows a frequency reading then it is running
Released for:Schneider Electric Nigeria
Explore more
Range:
Explore more
Range: