{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
Search FAQs
Can I get a graphic keypad for an ATV340?
Issue:
Customer needs a graphic keypad for an ATV340?

Product Line:
ATV340

Environment:
Keypad display

Cause:
N/A

Resolution:
The ATV340 drive can use the Plain Text Display Terminal VW3A1113.  It will be mounted directly to the front of the drive.  It can also be remote mounted using part number VW3A1114, and one of the cables listed below.
The ATV340 drive can also use the Graphic Display Terminal  VW3A1111 (also used on the Altivar Process Drives) which can be connected to the drive using the Remote mount kit (VW3A1112) and a cable

The cables to connect the display to the drive are:
1 Meter - VW3A1104R10
3 Meters - VW3A1104R30
5 Meters - VW3A1104R50
10 Meters - VW3A1104R100

NOTE: The drive does not come with either of these displays.  They must be ordered separately.
NOTE: Only one display can be connected to the drive.

Schneider Electric Nigeria