{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
Search FAQs
Can you run multiple motors with one ATV320 drive?

Article available in these languages: Czech, Japanese

Issue:
Trying to run multiple motors with one ATV320 drive.

Product Line:
ATV320

Environment:
Operating multiple motors simultaneously

Cause:
Documentation

Resolution:
Yes, but you need to size the drive according to the sum of the HP and max current of all the motors and provide separate overload protection for each motor.
All motors will will start/stop at the same time and run at the same speed.

Schneider Electric Nigeria