{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
Search FAQs
How can you do torque control over communications like Ethernet/IP on the ATV930 drive?
Issue:
ATV930 torque control over communications like Ethernet/IP

Product Line:
ATV930

Environment:
All

Cause:
Wants to write the torque reference over the network to control motor torque.

Resolution:
LTR address 8505 has to entered into the IO Scanner output table using Somove.

Schneider Electric Nigeria