{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
Search FAQs
Is the ATV31 drive compatible with Somove software?
Issue:
ATV31 drive compatibility with Somove.

Product Line:
Altivar 31

Environment:
All

Cause:
Software

Resolution:
Yes,  the ATV31 drives can be used with Somove software.
The DTM files for altivar drives will need to be installed as seen from link below.

DTM file for all other supported Altivar series drives:
https://www.se.com/ww/en/download/document/Altivar_DTM_Library

Schneider Electric Nigeria