Search FAQs
Is Metasys N2 communication protocol available for the Atlivar Process drives?
Issue:
Customer is replacing an old ATV61 drive with Metasys N2 card. Wants to be able to control and communicate to the drive using Metasys N2.
Product line:
Altivar Process, ATV630, ATV930,
Environment:
All
Cause:
Is there a cross refernce that includes Metasys N2
Resolution:
The Process Drives do not have a Metasys N2 Communication card available. Customer will need to use a third-party Modbus RTU to Metasys N2 gateway.
The Altivar 212 for Fan and Pump applications may be an option, as that drive does have integrated protocols including Metasys N2.
Customer is replacing an old ATV61 drive with Metasys N2 card. Wants to be able to control and communicate to the drive using Metasys N2.
Product line:
Altivar Process, ATV630, ATV930,
Environment:
All
Cause:
Is there a cross refernce that includes Metasys N2
Resolution:
The Process Drives do not have a Metasys N2 Communication card available. Customer will need to use a third-party Modbus RTU to Metasys N2 gateway.
The Altivar 212 for Fan and Pump applications may be an option, as that drive does have integrated protocols including Metasys N2.
Released for:Schneider Electric Nigeria
Explore more
Range:
Explore more
Range: