No, the Berger Lahr EXRDM3913/50NEA motor with ID number 52951045500 is a special customized version for the company W&H.
This type is proprietary and is reserved for the company W & H and can not be purchased from Schneider Electric.
The customer must contact the OEM machine builder Windmuller & Holscher for a spare EXRDM3913/50NEA motor with ID number 52951045500.
This type is proprietary and is reserved for the company W & H and can not be purchased from Schneider Electric.
The customer must contact the OEM machine builder Windmuller & Holscher for a spare EXRDM3913/50NEA motor with ID number 52951045500.
Released for:Schneider Electric Nigeria