Search FAQs
How can I connect to my ATV drive with SoMove through an M251MESE (with IP forwarding) ?
Network topology is as following :
- Subnetwork 192.168.10.x : PC with SoMove connected to M251MESE port 1
- Subnetwork 192.168.100.x : M251MESE port 2 connected to ATV600 (or any other ATV with ethernet port)
PC :
192.168.10.1
255.255.255.0
M251 Port1 :
192.168.10.51
255.255.255.0
"Enable IP forwarding" checkbox enabled
M251 Port2 :
192.168.100.51
255.255.255.0
ATV600 :
192.168.100.60
255.255.255.0
Gateway : 192.168.100.51
On PC side the following command has to be entered in command prompt :
route add 192.168.100.0 MASK 255.255.255.0 192.168.10.51
- Subnetwork 192.168.10.x : PC with SoMove connected to M251MESE port 1
- Subnetwork 192.168.100.x : M251MESE port 2 connected to ATV600 (or any other ATV with ethernet port)
PC :
192.168.10.1
255.255.255.0
M251 Port1 :
192.168.10.51
255.255.255.0
"Enable IP forwarding" checkbox enabled
M251 Port2 :
192.168.100.51
255.255.255.0
ATV600 :
192.168.100.60
255.255.255.0
Gateway : 192.168.100.51
On PC side the following command has to be entered in command prompt :
route add 192.168.100.0 MASK 255.255.255.0 192.168.10.51
Released for:Schneider Electric Nigeria
Explore more
Range:
Explore more
Range: