{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
Search FAQs
What are the internal consumption (burden) specification of the ION8650 IO expander module
Issue
Control power specifications of the ION8650 IO expander module

Product Line
ION8650

Environment
Metering application requiring control for the metering devices

Cause
Need to assess burden of IO expander module of the ION8650

Resolution
The power consumption of the 8650 IO Expander is around 2.5 W minimum (typical) and less than 5 W maximum.

Schneider Electric Nigeria