Search FAQs
AccuSine PCS+ Dual operation mode
Issue
The AccuSine+ can be used as a harmonic filter and power factor correction/Load balancing simultaneously. The total output current will be limited by harmonic current and the reactive current.
Product Line
AccuSine PCS+
Resolution
The total output of the harmonic filter in dual mode is governed by the following formula:
When the total current output of the active filter required exceeds the unit rating, the AccuSine PCS+ has a harmonic priority setting to determine which mode has priority.
Use percentage of harmonic priority to set output current split
The AccuSine+ can be used as a harmonic filter and power factor correction/Load balancing simultaneously. The total output current will be limited by harmonic current and the reactive current.
Product Line
AccuSine PCS+
Resolution
The total output of the harmonic filter in dual mode is governed by the following formula:
When the total current output of the active filter required exceeds the unit rating, the AccuSine PCS+ has a harmonic priority setting to determine which mode has priority.
Use percentage of harmonic priority to set output current split
- 100% means output capacity utilized for harmonic correction, then left over can be used for Power factor correction.
- 0% assigns fundamental (PF correction) current as the primary mode, left over used for harmonic correction.
Released for:Schneider Electric Nigeria
Explore more
Range:
Explore more
Range: