{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
Search FAQs
Can I display torques as 'Foot Pounds' on the ATV630 / ATV690 series drives?
Issue:
Change unit of torque to "Foot Pounds" on Altivar Process Drives ATV630/930

Product Line:
ATV630, ATV690 series drives.

Environment:
All models with firmware 1.6 or below.

Cause:
Information unavailable in current literature.

Resolution:
Currently, it is not possible to display torque as foot pounds on the ATV630 and ATV930 series drives.  This information is current as of firmware release 1.6.  An evolution has been created to have this feature added via a future firmware update.  There is no ETA for this firmware release.

Schneider Electric Nigeria