{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
Search FAQs
PM55xx series firmware Version 2.4.3, and release notes
Issue
Customer is looking for a new firmware upgrade

Product Line
PM5500 Series Meters

Environment
Firmware upgrade

Cause
Customer needs to upgrade PM5500 series meter upgrade

Resolution
RELEASE NOTES:

PM55xx firmware upgrade to address bug fixes, performance, and new features.

Updates:

New Features
DPWS feature: Allows self-discovery of the meter when connected in Local Area Network
•    Added MAC Address within the display of the HMI.
Corrections
•    Webpage new user password not stored at first time: Fixed
•    Watch dog timer implemented to address communication loss

Additional fixes
This firmware update is intended for PowerLogic PM5560 / PM5563 Basic Power Meters.

Direct Firmware Links:
Please see attached below: PM5560_PM5563_V2.4.3.zip

How to upgrade PM55xx firmware:
Please see FA299853.

Schneider Electric Nigeria

Attachment(s)
PM5560_PM5563_V2.4.3.zip [1.81 MB]