{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
Search FAQs
What are the communication protocols supported by the power meter PM5560 with the reference METSEPM5560 ?
The communication protocols supported by the power meter PM5560 with the reference METSEPM5560 are as follows:

Modbus RTU and ASCII 2 wires with RS485 port, : 9.6, 19.2 and 38.4 kbauds, even/odd or none, insulation: 2500 V, JBUS
Modbus TCP/IP : 10/100 Mbit/s, insulation: 2500 V
Ethernet Modbus TCP/IP daisy chain with Ethernet port
BACnet IP

Schneider Electric Nigeria