{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
Search FAQs
How a user can change Demand Setup on PM5310 meter
Customer want to know how he can change Demand Setup on PM5310 meter.
PM5000, any of them including those which have Ethernet card, are serial meters with under a TCP/IP access point.
Customer should use an Ethernet gateway like EGX wire PM5310 serial meter under RS485 port of EGX and ION Setup in Network mode to do meter PM5310 setup.
Mind that the meter PM5310 do not log Power but it do Power Demand calculation. This is say into document EAV15107 - EN04_PM5300 - PowerLogic™ PM5300 series user guide Chapter 9—Measurements and calculations, page 79, Power demand calculation methods.
User can configure the power demand calculation method from the front panel or using ION Setup.
Attached is a guide to create a network under ION Setup and access Demand Settings of PM5300 meter.

Schneider Electric Nigeria

Attachment(s)
Use ION Setup to access PM5310 Demand settings.zip [491.73 KB]