{}

Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
How can we help you today?
On a ATV320 drive, what would cause register 5202, reading logic input status LI6, not to turn on?
Issue:
Register 5202, reading logic input status LI6, is not to turning on when the input is energized.

Product Line:
ATV320 drive

Environment:
All 

Cause:
LI6 status is not showing up on register 5202 logic input status. 

Resolution:
Reading address 5202 over Canopen or modbus and bit 5 for LI6 is not turning on. 

When inputs are wired for SOURCE;
Verify the SW1 switch is in SOURCE position.
Verify the input by measuring LI6 - COM for 24Vdc.  
Verify the SW2 switch is in DI6 position.

Schneider Electric Nigeria

Explore more
Range:
Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.
Explore more
Range:
Your browser is out of date and has known security issues.

It also may not display all features of this website or other websites.

Please upgrade your browser to access all of the features of this website.

Latest version for Google Chrome, Mozilla Firefox or Microsoft Edgeis recommended for optimal functionality.