{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
Search FAQs
Can the ATV600 live stream data from the data log?
Issue:
Customer wants to stream data captured by the Data logger in real time.

Product Line:
ATV600 ATV900 Process drives

Environment:
All models, All serial numbers

Cause:
Function not defined in the manual

Resolution:
It is not possible to stream data from the drive via the data logger.  The Data logger was designed to capture samples of data and make them available for download via SoMove software.

Schneider Electric Nigeria