{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
Search FAQs
Downgrading a BMXCRA31210 firmware with less than v2.18 can cause some Ethernet ports not to function
Issue
This Resolution describes why there is a minimum firmware version of 2.18 for a BMXCRA31210 at a PV07.
Some Ethernet ports of a BMXCRA31210, at a PV07 or higher, will not function if the firmware is downgraded to any version less than 2.18

Product Line
BMXCRA31210   PV07

Resolution
  • Firmware version 2.18 was created to operate with the new PV07 module and is compatible with previous PV versions.
  • Firmware version 2.18 has the exact same functionality as version 2.16.  There are no fixes and no improvements.  The requirement for firmware version 2.18 was due to a component change in PV07 and higher modules.
  • BMXCRA31210 modules at PV07 are not compatible with firmware versions less than 2.18.






Schneider Electric Nigeria