Search FAQs
What network protocols are standard embedded in an ATV630 Process drive?
Issue:
Network protocols embedded in the standard ATV630 Process drive.
Product Line:
Altivar 630, Process
Environment:
All
Cause:
Communications
Resolution:
The ATV630 drive has embedded Modbus TCP (ethernet) and Modbus RTU (RJ45).
Network protocols embedded in the standard ATV630 Process drive.
Product Line:
Altivar 630, Process
Environment:
All
Cause:
Communications
Resolution:
The ATV630 drive has embedded Modbus TCP (ethernet) and Modbus RTU (RJ45).
Released for:Schneider Electric Nigeria
Explore more
Range:
Explore more
Range: