Search FAQs
Connecting an EGX150 to a serial RS485
Issue
The Serial port for the EGX150 uses an RJ45 connector, which is different from the standard RS-485 connector.
Product Line
Link150, EGX150
Environment
EGX150 serial connections
Cause
The EGX150 does not use the standard RS-485 connector.
Resolution
Connect, using a straight through RJ45 cable to the RS-485 port on your EGX150.
Cut the other end (that is to be connected to your slave device) to expose the wires.
2-Wire RS-485 connection:
Use the Blue wire as the positive (+) and the Blue/White striped wire as the negative (-)
![](https://ckm-content.se.com/ckmContent/servlet/servlet.ImageServer?id=0151H000009I2RzQAK&oid=00DA0000000abSm)
4-Wire RS-485 connection:
![](https://ckm-content.se.com/ckmContent/servlet/servlet.ImageServer?id=0151H000009I2S0QAK&oid=00DA0000000abSm)
Kindly refer to the EGX150 User Guide for details on how to wire the RS-485 port.
The Serial port for the EGX150 uses an RJ45 connector, which is different from the standard RS-485 connector.
Product Line
Link150, EGX150
Environment
EGX150 serial connections
Cause
The EGX150 does not use the standard RS-485 connector.
Resolution
Pin Number | Colour | Signal name | Description |
---|---|---|---|
1 | Orange/White striped | Rx- | Receive Data - |
2 | Orange | Rx+ | Receive Data + |
3 | NC | No Connection | |
4 | Blue | Tx+ | Transmit Data + |
5 | Blue/white striped | Tx- | Transmit Data - |
6 | NC | No Connection | |
7 | NC | No connection | |
8 | GND | Ground |
Connect, using a straight through RJ45 cable to the RS-485 port on your EGX150.
Cut the other end (that is to be connected to your slave device) to expose the wires.
2-Wire RS-485 connection:
Use the Blue wire as the positive (+) and the Blue/White striped wire as the negative (-)
4-Wire RS-485 connection:
RJ45 Pin Number | Master | Slave |
---|---|---|
1 | Rx- | Tx- |
2 | Rx+ | Tx+ |
4 | Tx+ | Rx+ |
5 | Tx- | Rx- |
Kindly refer to the EGX150 User Guide for details on how to wire the RS-485 port.
Released for:Schneider Electric Nigeria
Explore more
Range:
Explore more
Range: