Search FAQs
Can you read speed as a percent via thru ethernet on the ATV630 and ATV930 process drives?
Issue:
Can you read speed as a percent via thru ethernet on the process drives?
Product Line:
ATV630 and ATV930 drives
Environment:
All
Cause:
Wants to read the drive as a percent vs rpms
Resolution:
The speed is only in “rpm” (SPD parameter) or “Hz” (RFR parameter), there is no other speed parameter in “%”.
If the drive is controlled by a PLC, then it’s possible to convert the speed in “%” with the PLC.
If the point is to display the speed in “%” on the keypad, then it’s not possible customize displayed parameters, only parameters which are in “Complete Settings”.
I have created a request (PEP0405819R) in order to customize all parameters and so parameters in “Display” menu.
Can you read speed as a percent via thru ethernet on the process drives?
Product Line:
ATV630 and ATV930 drives
Environment:
All
Cause:
Wants to read the drive as a percent vs rpms
Resolution:
The speed is only in “rpm” (SPD parameter) or “Hz” (RFR parameter), there is no other speed parameter in “%”.
If the drive is controlled by a PLC, then it’s possible to convert the speed in “%” with the PLC.
If the point is to display the speed in “%” on the keypad, then it’s not possible customize displayed parameters, only parameters which are in “Complete Settings”.
I have created a request (PEP0405819R) in order to customize all parameters and so parameters in “Display” menu.
Released for:Schneider Electric Nigeria
Explore more
Range:
Explore more
Range: