{}

Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
How can we help you today?
Vijeo Designer v6.2 crashed with a Unhandled Exception Error when launched within Somachine v4.2 with Windows 10 Pro. How to resolve the issue?
Issue:
Vijeo Designer v6.2 crashed with a Unhandled Exception Error when launched within Somachine v4.2 with Windows 10 Pro.  How to resolve the issue?

Product Line:
Vijeo Designer, Somachine v4.2, Windows 10, Unhandled Exception Error 

Resolution:
If you are getting the following errors in the log file:
[2017-08-10 07:39:05:7138] CM: OnAssemblyResolve: Failed to load assembly 'SchneiderElectric.Central.Gui.Common.Items' (main assembly failed to load)
[2017-08-10 07:39:08:4222] CM: OnAssemblyResolve: Failed to load assembly 'DocExport, Version=3.5.6.0, Culture=neutral, PublicKeyToken=null' (redirecting into the Common folder was not successful)
[2017-08-10 07:39:12:281] CM: OnAssemblyResolve: Failed to load assembly 'SchneiderElectric.Central.Common.XmlSerializers, Version=1.55.14.0, Culture=neutral, PublicKeyToken=null' (redirecting into the Common folder was not successful)
[2017-08-10 07:39:12:2815] CM: OnAssemblyResolve: Failed to load assembly 'SchneiderElectric.Central.Common.XmlSerializers' (main assembly failed to load)
[2017-08-10 07:39:12:6181] CM: OnAssemblyResolve: Failed to load assembly 'SchneiderElectric.Central.Gui.Resources.resources, Version=1.55.14.0, Culture=en-US, PublicKeyToken=null' (matching main assembly not found)
[2017-08-10 07:39:12:6206] CM: OnAssemblyResolve: Failed to load assembly 'SchneiderElectric.Central.Gui.Resources.resources, Version=1.55.14.0, Culture=en-US, PublicKeyToken=null' (matching main assembly not found)

If the error in the log file has to do with loading the SoMachine PlugIns components (as above).
Delete the cache files *.cache  which can be found under folder "C:\ProgramData\AP\PlugInCaches", and afterward start SoMachine and retest.

Keep in mind that the folder C:\ProgramData is a hidden folder so you will not see, by default setting inside the windows explorer

If the problem still exist, please contact Schneider Electric Technical Support and open a ticket.

Schneider Electric Nigeria

Explore more
Range:
Your browser is out of date and has known security issues.

It also may not display all features of this website or other websites.

Please upgrade your browser to access all of the features of this website.

Latest version for Google Chrome, Mozilla Firefox or Microsoft Edgeis recommended for optimal functionality.