Search FAQs
What is the Syntax to access a symbol using the OPCXML-DA
Issue
Provide the syntax to use for accessing a symbol using OPCXML-DA.
Product Line
OFS
Environment
Windows 10
Resolution
The following exampledemonstrate how to directly access a symbol in a PLC using OPCXML-DA. The symbol in the PLC
can be accessed by OFS using either the 'Data Dictionary' or the '.XVM' file method. It is accomplished using the OPC property
'ItemPath' and 'ItemName'.
e.g.,
Given the following:
The syntax to directly access the the symbol using OPCXML-DA is:defined as:
http://stationname/Website/OFS/ws/OPCXMLDa.asmx/myAlias!CPU227OPC
Provide the syntax to use for accessing a symbol using OPCXML-DA.
Product Line
OFS
Environment
Windows 10
Resolution
The following exampledemonstrate how to directly access a symbol in a PLC using OPCXML-DA. The symbol in the PLC
can be accessed by OFS using either the 'Data Dictionary' or the '.XVM' file method. It is accomplished using the OPC property
'ItemPath' and 'ItemName'.
e.g.,
Given the following:
- The Alias for the device name in in OFS is defined as 'myAlias'
- The symbol name in the Unity application is defined as 'CPU227OPC'
- ItemPath= "http://stationname/Website/OFS/ws/OPCXMLDa.asmx"
- ItemName= myAlias!CPU227OPC
The syntax to directly access the the symbol using OPCXML-DA is:defined as:
http://stationname/Website/OFS/ws/OPCXMLDa.asmx/myAlias!CPU227OPC
Released for:Schneider Electric Nigeria
Explore more
Range:
Explore more
Range: