Video: How to configure Unity Momentum USB connection with the RNDIS driver if it does not show up in the network connections.
If the RNDIS driver does not show up as available you will need to go to network connections and edit the IP address to 90.0.0.2. The following video demonstrates this procedure:
Released for:Schneider Electric Nigeria
Explore more
Range:
Modicon M221
Articles that might be helpful
Show more articles
Discuss this topic with experts
Visit our Community for first-hand insights from experts and peers on this topic and more.