{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
Search FAQs
How do you read the serial number on the ATV320 drives?
Issue:
ATV320 Serial number break down

Product Line:
ATV320 and ATV340

Environment:
All

Cause:
Needs to read the date code.

Resolution:
The  serial number for the ATV320 is like example  HL1610858003

HL= Manufacturing location
16= year 2016
10= week 10

This serial number is located at the bottom right side of the gray sticker under the bar code.

Schneider Electric Nigeria