Search FAQs
Is it possible to replace coil in S207 contactors for railway applications?
The S207 series contactors for railway applications use specific plastic to be compliant with EN45545 standard.
Therefore, standard coils (e.g. LX4D7SW) cannot be used because they are not using the specific plastic.
We do not have any spare part coil reference for S207 contactors.
Therefore, standard coils (e.g. LX4D7SW) cannot be used because they are not using the specific plastic.
We do not have any spare part coil reference for S207 contactors.
Released for:Schneider Electric Nigeria
Explore more
Range:
Explore more
Range: