Issue:
ATV320 usage of option cards
Product line:
Altivar 320, ATV320
Environment:
All
Cause:
Installation
Resolution:
Altivar Machine ATV320 drives are designed for use with option modules according to machine and application requirements. One option module can be used with an Altivar Machine ATV320 at a time. The option modules are compatible with all Altivar Machine ATV320 drives.
NOTE - The VW3A3600 option module adapter is required to connect an option module to compact-style Altivar Machine ATV320 drives (part numbers that end with a "C" , ATV320...C).
ATV320 usage of option cards
Product line:
Altivar 320, ATV320
Environment:
All
Cause:
Installation
Resolution:
Altivar Machine ATV320 drives are designed for use with option modules according to machine and application requirements. One option module can be used with an Altivar Machine ATV320 at a time. The option modules are compatible with all Altivar Machine ATV320 drives.
NOTE - The VW3A3600 option module adapter is required to connect an option module to compact-style Altivar Machine ATV320 drives (part numbers that end with a "C" , ATV320...C).
Released for:Schneider Electric Nigeria