{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.

Search FAQs

What is the difference between LRD** and LR3D** relays?

LR3D** relays are used for the unbalanced loads : there can be different currents in the three phases of the overload relay ( according to its size ) . examples : distribution circuits which have not the same loads on each phases, or single phase motor. This relay will not trip if the currents in its phases are different.
The LRD** which is for balanced load : that means with the same current on the three phases ( e.g. a squirrel cage motor ).
This is the only difference between LRD & LR3D relay.

Schneider Electric Nigeria