{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
Search FAQs
Video: How to change control terminal type from sink to source or from source to sink on ATV61/71 drives?
Issue:
Configuring Sink Mode on Altivar 61 & 71 Drives.

Product Line:
Altivar 61
Altivar 71

Environment:
All

Cause:
Terminal control mode configuration

Resolution:
First, to get access to the control terminals, open the cover on the control front panel.
Undo the locking screw until the spring is full extended.
Remove the card by sliding it downwards.
Note the SW1 switch on the card.
Move the DIP switch accordingly.
Reseat the card back into its slot and re-tighten the locking screw.
SW1

Schneider Electric Nigeria