{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
Search FAQs
STMSDK COM object initialization error when starting Unity after installing PES

Issue
STMSDK COM object initialization error when starting Unity after installing PES

Product Line
Unity

Environment
Windows 10

Resolution
Attempts to start Unity after installing PES returns the message ' Error when initializing programming unit (STMSDK COM object initialization):
Unexpected exception (memory allocation, ...

This error will appear if the 'Visual C++ Redistributable for Visual Studio 2012 Update 4' is corrupted.  To resolve the issue, re-install or repair
the 'Visual C++ Redistributable for Visual Studio 2012 Update 4'

The installation files for the 'Visual C++ Redistributable for Visual Studio 2012 Update 4' can be downloaded from:
https://www.microsoft.com/en-us/download/details.aspx?id=30679

Schneider Electric Nigeria