{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
Search FAQs
What would cause the ATV630 process drives fault relay not to change state after the external fault is activated?
Issue:
Cause of fault relay not changing state after the external fault is activated on the ATV630.

Product Line:
ATV630 and ATV930

Environment:
All

Cause:
The auto restart is preventing the relay from changing until the timeout is over.

Resolution:
The auto restart will prevent the fault relay from turning on until after the auto start time delay.

Schneider Electric Nigeria