{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.

Search FAQs

How to use a Thermocouple with the ABE-7CPA412?

Issue
How to use a Thermocouple with the ABE-7CPA412 for the BMXART0414 or BMXART0814?

Product Line
Telefast, x80 IO

Environment
ABE-7CPA412, BMXART0414, BMXART0814

Resolution
Telefast ABE-7CPA412 has an internal cold junction compensation to Thermocouple compatible with BMXART0414/BMXART0814. So, it is very important to know how to wire it when the channel is configured for thermocouple with the Telefast cold junction compensation in Unity Pro/Control Expert (as the pictures below).


Schneider Electric Nigeria

Explore more
Range:
Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.
Explore more
Range: