{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
Search FAQs
How to troubleshoot a TeSys T Long Start Fault
Issue:
Why is the TeSys T showing a long start fault when trying to run the motor?

Product Line:
TeSys T Motor Management Controller

Environment:
Products sold in the North American Market

Cause:
Installation / Troubleshooting

Resolution:
The TeSys T comes with Long Start Fault set as a default to trip after 10 seconds if the FLA of the motor has not come down to less than 100% of the FLC1 setting.
If experiencing nuisance tripping, first check that FLC1 is set to match the nameplate motor full load current.
If the FLC1 setting is set correctly it could be that you need longer to come down below FLA, first try setting long start to 15 seconds, if this does not work you can try 20 seconds. Once you reach a time that does not experience nuisance tripping you can start dialing back down the time until you experience nuisance tripping again to make the setting more precise.
If you do not need long start protection you can also disable this fault.

Schneider Electric Nigeria

Explore more
Range:
Product:
Articles that might be helpful Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.
Explore more
Range:
Product: