Issue:
Can I use Bonitron unit connected on the DC bus to power up the ATV320 drive?
Product Line:
ATV320, Altivar 320
Environment:
All
Cause:
Customer has 1-phase line power.
Resolution:
Technically, if the Bonitron unit is sized properly, it could work. However, We have not tested that combination, and we have no UL listing on it.
Can I use Bonitron unit connected on the DC bus to power up the ATV320 drive?
Product Line:
ATV320, Altivar 320
Environment:
All
Cause:
Customer has 1-phase line power.
Resolution:
Technically, if the Bonitron unit is sized properly, it could work. However, We have not tested that combination, and we have no UL listing on it.
Released for:Schneider Electric Nigeria