{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
Search FAQs
Video: How to Start your Symmetra PX 250/500 UPS

Article available in these languages: Spanish

Issue:
How to Start your Symmetra PX 250/500 UPS

Product line:
Symmetra PX 250/500

Environment:
All Product models, all serial numbers

Resolution:
Begin by applying power to the UPS by Closing the Q1 Breaker (Located in System I/O Cabinet)



Once the display is completely powered up and the Home screen is displayed, press the wrench icon in the lower left of the screen



Then select the operation button
Select System Startup



Follow the on screen prompts for starting up the UPS.  As each option is performed it will highlight the next step.


Some options are automated and will be done for you.

The following video demonstrates this procedure:

Schneider Electric Nigeria