{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
Search FAQs
What would cause the customers Ethernet switch to not allow the ATV630 and ATV930 drives single Ethernet port connections?
Issue:
Possible cause that Ethernet switch not allowing the ATV630/930 drives single Ethernet port connections.

Product Line:
ATV630 and ATV930 using Ethernet and only one of the two parts are used like in a star configuration.

Environment:
All

Cause:
Rapid spanning tree for the Ethernet port is active.

Resolution:
Using somove you will need to turn off the RSTP under the Ethernet settings to allow the singe Ethernet connection to the switch.

RSTP

Schneider Electric Nigeria