{}

Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
Search FAQs
Which ATV340 Drives have embedded Ethernet protocol.

Article available in these languages: Turkish


There is no option to add an Ethernet option on the non E suffix ATV340 drives.  If the Ethernet port on the ATV340.....E  fails you can not replace the module its not replaceable.  The non E suffix version or Standard ATV340 does support modbus but not Modbus TCP.

Only the E version of the ATV340.....E   drive supports Both Modbus TCP and Ethernet IP.
On a side note only the none E suffix version allow the other option cards not the E suffix version. 
1:) CANopen
2: )PROFIBUS DP V1
3:) DeviceNet
4:) EtherCAT
5:) ProfiNet

Schneider Electric Nigeria

Explore more
Range:
Your browser is out of date and has known security issues.

It also may not display all features of this website or other websites.

Please upgrade your browser to access all of the features of this website.

Latest version for Google Chrome, Mozilla Firefox or Microsoft Edgeis recommended for optimal functionality.