{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
Search FAQs
What would cause the ATV630 Ethernet IP option card VW3A3720 to not show up in somove under the Fieldbus A slot?
Issue:
Causes for an ATV630 Ethernet IP option card VW3A3720 to not show up in somove under the Fieldbus A slot.

Product Line:
ATV630 with

Environment:
All

Cause:
ATV630 drives firmware is not at 1.5 or greater or you may need to build a project offline and then import the program into Somove.

Resolution:

Checked option 1 and it shows Ethernet IP card.  option 2 is no
Drive firmware is Version 1.5IEXX  or greater  which is good for the Ethernet IP option card.

Next Open up the Somove software:

Checked and we created a project offline adding the Ethernet IP card for option A

Now we copied the program from the drive and now it shows up as Ethernet IP under slot A in the Field bus section under Parameter list.

Schneider Electric Nigeria