{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
Search FAQs
Video: Back-UPS Pro M2 & RS with SineWave; Adjustment of unit battery transfer sensitivity

Article available in these languages: Spanish

Issue:
APC
Back-UPS Pro M2 & RS with SineWave; Adjusting the battery transfer settings.

Product Line:

Back-UPS Pro "M2" and "BR SineWave" models
BR1000MS / BN1100M2 / BN1350M2 / BR1350MS / BN1500M2 / BR1500MS

Cause:
UPS is not operating On-line or may be transferring to battery power frequently.

Resolution:
The following video details the process for manually adjusting the on-battery transfer thresholds for the Back-UPS Pro M2 & RS with SineWave series. These settings may also be adjusted through PowerChute Personal Edition software on compatible Windows computers.

Schneider Electric Nigeria