{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.

Search FAQs

Video: Connecting the Unity DTM Browser to the BMENOC0301 module

Issue
Establishing a connection between the Unity Pro DTM Browser to the Modicon M580 BMENOC0301 Ethernet Module.

Product Line
M580 BMENOC0301

Environment

Control Expert DTM Browser

Resolution
Below is a video that shows how to setup the Unity DTM Browser to connect to the BMENOC0301 module.
Connectivity requires the selection of the correct Source IP Address (PC) that will be used by Unity to connect.

Schneider Electric Nigeria

Explore more
Range:
Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.
Explore more
Range: