Issue:
Setting the timeout on the ATV71 drive using IO scanner and Ethernet TCP-IP
Product Line:
ATV71
Environment:
All
Cause:
Loss of communications from the Ethernet.
Resolution:
If the customer needs to change the time out for Ethernet communications he can do it from the web page or the (Tout) parameter in the drive.
The default is 2 seconds.
See the attachment.
Setting the timeout on the ATV71 drive using IO scanner and Ethernet TCP-IP
Product Line:
ATV71
Environment:
All
Cause:
Loss of communications from the Ethernet.
Resolution:
If the customer needs to change the time out for Ethernet communications he can do it from the web page or the (Tout) parameter in the drive.
The default is 2 seconds.
See the attachment.
Released for:Schneider Electric Nigeria
Did this answer your question?
Issue:
Setting the timeout on the ATV71 drive using IO scanner and Ethernet TCP-IP
Product Line:
ATV71
Environment:
All
Cause:
Loss of communications from the Ethernet.
Resolution:
If the customer needs to change the time out for Ethernet communications he can do it from the web page or the (Tout) parameter in the drive.
The default is 2 seconds.
See the attachment.
Setting the timeout on the ATV71 drive using IO scanner and Ethernet TCP-IP
Product Line:
ATV71
Environment:
All
Cause:
Loss of communications from the Ethernet.
Resolution:
If the customer needs to change the time out for Ethernet communications he can do it from the web page or the (Tout) parameter in the drive.
The default is 2 seconds.
See the attachment.
Released for:Schneider Electric Nigeria
Did this answer your question?
Issue:
Setting the timeout on the ATV71 drive using IO scanner and Ethernet TCP-IP
Product Line:
ATV71
Environment:
All
Cause:
Loss of communications from the Ethernet.
Resolution:
If the customer needs to change the time out for Ethernet communications he can do it from the web page or the (Tout) parameter in the drive.
The default is 2 seconds.
See the attachment.
Setting the timeout on the ATV71 drive using IO scanner and Ethernet TCP-IP
Product Line:
ATV71
Environment:
All
Cause:
Loss of communications from the Ethernet.
Resolution:
If the customer needs to change the time out for Ethernet communications he can do it from the web page or the (Tout) parameter in the drive.
The default is 2 seconds.
See the attachment.