{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
Search FAQs
What is the possibility of using Zone Selectivity Interlocking (ZSI) between upstream (NSX160-250) & downstream (NSX160-250)?
To use the ZSI function between 2 Compact NSX MCCBs; one in the upstream and the other in the downstream, one of them will have to be a Compact NSX400~630 to contain the terminals Z3, Z4 and Z5. These terminals are the ones to which the downstream MCCB should be connected to. Compact NSX100~250 MCCBs do not contain these terminals (Z3, Z4 and Z5) and thus won't be able to perform the ZSI function if placed in the upstream/downstream combinations. Please refer to the attached pages from the Micrologic trip unit user manual (refer to "Extract - Compact NSX - Micrologic 5 or 6 - User manual.pdf"). So to make use of the ZSI function between 2 Compact NSX MCCBs, please make that the upstream breaker is Compact NSX400~630.

Schneider Electric Nigeria

Attachment(s)
Extract - Compact NSX - Micrologic 5 or 6 - User manual.pdf [197.17 KB]