{}

Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
Search FAQs
How does the Reset button work on the TeSys T?

Issue:
Identify the functioning of the TeSys T's reset button

Product Line:
IEC Overload Relays

Environment:
Products sold in the US

Cause:
Resetting a fault on an LTMR

Resolution:

The reset button on the front of the TeSys T LTMR controller can be used to reset a fault, perform a self test, return the device to factory default settings, or induce a fault.

To reset a fault press the button and release it within 3 seconds.
To perform a self test, Press and hold the button for 3 to 15 seconds.
To perform a Full Factory Reset of the Tesys, press and hold the button for 15 to 20 seconds. (This will clear the programming in the Tesys T and return the programming to 'factory new' state).
To generate a fault condition, press and hold the button for more than 20 seconds.  Note that a fault created by holding the Reset button in for more than 20 seconds will require a power cycle to reset.  It can not be reset by pressing the reset button and releasing it within 3 seconds.


Schneider Electric Nigeria

Explore more
Range:
Your browser is out of date and has known security issues.

It also may not display all features of this website or other websites.

Please upgrade your browser to access all of the features of this website.

Latest version for Google Chrome, Mozilla Firefox or Microsoft Edgeis recommended for optimal functionality.