Issue
Does WSOS V5 software support Windows 10?
Product Line
WSOS
Environment
Reclosers
Resolution
Version 5.16XX has support for Windows 7 and above, so it will work for Windows 10.
This is from page 6 of the release notes of the software
"Release version 5.16.xx of the Windows Switchgear Operating System allows the users to install and run the engineering tool on Microsoft Windows®10 operation system, which was not possible with the previous WSOS version 5.15.xx.
There is no change to the installation process. Double clicking on the installer and following the instructions on the installation wizard screen will guide the user as required.
The same version can be installed on Microsoft Windows 7 or Microsoft Windows 8 Operating systems as well."
Does WSOS V5 software support Windows 10?
Product Line
WSOS
Environment
Reclosers
Resolution
Version 5.16XX has support for Windows 7 and above, so it will work for Windows 10.
This is from page 6 of the release notes of the software
"Release version 5.16.xx of the Windows Switchgear Operating System allows the users to install and run the engineering tool on Microsoft Windows®10 operation system, which was not possible with the previous WSOS version 5.15.xx.
There is no change to the installation process. Double clicking on the installer and following the instructions on the installation wizard screen will guide the user as required.
The same version can be installed on Microsoft Windows 7 or Microsoft Windows 8 Operating systems as well."
Released for:Schneider Electric Nigeria
Issue
Does WSOS V5 software support Windows 10?
Product Line
WSOS
Environment
Reclosers
Resolution
Version 5.16XX has support for Windows 7 and above, so it will work for Windows 10.
This is from page 6 of the release notes of the software
"Release version 5.16.xx of the Windows Switchgear Operating System allows the users to install and run the engineering tool on Microsoft Windows®10 operation system, which was not possible with the previous WSOS version 5.15.xx.
There is no change to the installation process. Double clicking on the installer and following the instructions on the installation wizard screen will guide the user as required.
The same version can be installed on Microsoft Windows 7 or Microsoft Windows 8 Operating systems as well."
Does WSOS V5 software support Windows 10?
Product Line
WSOS
Environment
Reclosers
Resolution
Version 5.16XX has support for Windows 7 and above, so it will work for Windows 10.
This is from page 6 of the release notes of the software
"Release version 5.16.xx of the Windows Switchgear Operating System allows the users to install and run the engineering tool on Microsoft Windows®10 operation system, which was not possible with the previous WSOS version 5.15.xx.
There is no change to the installation process. Double clicking on the installer and following the instructions on the installation wizard screen will guide the user as required.
The same version can be installed on Microsoft Windows 7 or Microsoft Windows 8 Operating systems as well."