{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
Search FAQs
What is the Efficiency of the EV Link Chargers?
1) Inside EV Link a mother board with a 24V power supply commanding a contact is installed.
2) Less than 100W of consumption when the CT is closed. We are just a gate between the grid and the car.

So the maximum consumption is 100w (dedicated to 24v power supply, motherboard, contactor and led). Efficiency will be,
If the load is a 3,7kW (16A 1P) efficiency = 97%
If the load is a 22kW (32A 3P) efficiency = 99,5%

But, also consider the Harmonics, Power factor produced by the Car itself which will affect efficiency.

Schneider Electric Nigeria

Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.