Search FAQs
Why am I unable to discover the Enerlin'X devices within my smartpanel with the Masterpact MTZ connected after performing the Automatic Trip Curve Test using Ecoreach?
Issue: Unable to discover the Enerlin'X devices like the IO, IFE etc after running the Automatic Trip Curve test using Ecoreach.
Cause: The Automatic Trip Curve Test from Ecoreach was aborted in between and the Masterpact MTZ Control Unit (micrologic X) is still in Test Mode.
Resolution: 1) Bring the Micrologic X out of the Test Mode, this can be achieved by removing the USB cable connected between the Micrologic X and computer with Ecoreach installed and reconnecting. Now, the Enerlin'X devices will be discovered by Ecoreach.
2) Wait for 15 minutes, the Micrologic X will be automatically out of test mode.
Cause: The Automatic Trip Curve Test from Ecoreach was aborted in between and the Masterpact MTZ Control Unit (micrologic X) is still in Test Mode.
Resolution: 1) Bring the Micrologic X out of the Test Mode, this can be achieved by removing the USB cable connected between the Micrologic X and computer with Ecoreach installed and reconnecting. Now, the Enerlin'X devices will be discovered by Ecoreach.
2) Wait for 15 minutes, the Micrologic X will be automatically out of test mode.
Released for:Schneider Electric Nigeria
Explore more
Range:
Explore more
Range: