{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.

Search FAQs

What is a safety shutter and what are its features.

Safety shutter is mounted on the chassis of Easypact MVS/Masterpact NT/NW ACB, the safety shutters automatically block access to the
disconnecting contact cluster when the device is in the disconnected or test positions
(degree of protection IP 20) When the device is removed from its chassis, no live
parts are accessible.

The shutter-locking system is made up of a moving block (optional device) that can
be padlocked (padlock not supplied). The block:
>Prevents connection of the device
>Locks the shutters in the closed position

Schneider Electric Nigeria

Explore more
Range:
Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.
Explore more
Range: