{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.

Search FAQs

How we can see CT Connection Reversal with EM1000 or EM1200 or EM1220 display ?

CT Connection Reversal
To check the polarity of the CT after the meter has been installed, go to the DIAG (diagnostic) pages and check the CT REV display page. Refer to “EM1000/EM1200/EM1220 Power and Energy Meters Menu Hierarchy” on  for more information.
Assuming that you are consuming power (import), check for one of the following conditions in the meter:
1. If the display shows L 1 or L 2 or L 3, then CT phase 1 or CT phase 2 or CT phase 3 is reversed and the corresponding CT phase must be corrected.
2. If the display shows L 12 or L 23 or L 32, then CT phases (1 and 2) or CT phases (2 and 3) or CT phases (3 and 1) are reversed and the corresponding CT phases must be corrected.
3. If the display shows L 123, then all the phases are reversed and must be corrected.
4. If the display shows L-, then no CTs are reversed.

Schneider Electric Nigeria

Attachment(s)

CT connection Reversal _EM1000 _EM1200_EM1220.pdfCT connection Reversal _EM1000 _EM1200_EM1220.pdf [74.64 KB]
Explore more
Product:
Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.
Explore more
Product: